ATV61 or ATV71 Modbus Card part number
Issue:
What is the part number for ATV61 or ATV71 Modbus/Unitelway Option Card?

Product Line:
ATV61, ATV71

Environment:
All

Cause:
NA

Resolution:
The part number is VW3A3303. However, the card is obsolete.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj