How to modify Original WebX initial screen images and top left link
DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.

The initial screen of the Original WebX contains an image at the center of the screen ("logo.pnj") and a top left image ("headerleft.png") that can be customized. The top left image also has a hyperlink, originally leading to "http://www.schneider-electric.com" that can be customized as well:



Those files are located at "C:\Program Files\Schneider Electric\ClearSCADA\WWW\Images":



The end user can design and create their own image files and paste them to this same folder, for example "Mylogo.png" and "Myheaderleft.png":



Now the "C:\Program Files\Schneider Electric\ClearSCADA\WWW\XSL\layout.xsl" file must be changed to use the new images and a new link.
Find the following lines:
............................. .........................................................................................



And modify accordingly:

..........................................................................................................................



Save the changes. The result, in this example, would be (you may need to clear the browser cache in order to load the new images):



Note: Any changes on the original WebX files will be overwritten by an upgrade. You may want to save the modified files on a safe place so you can reuse them after an upgrade.







Schneider Electric Sverige