Sverige

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.

Du kan välja ett annat land för att se tillgängliga produkter eller gå till vår globala webbplats för information om företaget.

Välj ett annat land eller region

  • What you need to make a sustainable solar investment

Default Alternative Text
With the right balance-of-system solution, a PV power plant can earn a great ROI. More than 3 GW The combined capacity of large 3-phase inverters installed worldwide by Schneider Electric.

The key to earning a healthy ROI on your utility-scale solar project

A balance-of-system solution integrates everything needed to efficiently distribute and manage locally generated solar energy, from panel DC output to the grid connection. A Schneider Electric balance-of-system solution typically includes the following:

  • PV Box: an optimized power conversion system that can be fully tailored for specific needs or deployed as a standard solution brick, reducing installation time and costs.
  • Conext Core XC grid-tie inverters: the core of the PV power conversion system, a 3-phase inverter with best-in-class peak efficiency (98.9%) and fully configurable, grid-interactive features.
  • Array Boxes: a robust string combiner box that enables the connection of multiple PV module strings while protecting and monitoring the installation.
  • Grid-tie Substations: an HV or MV substation that ties the installation to the grid in compliance with local codes and regulations.

Conext Control monitoring and control solution: a single, standardized solution that integrates process, supervision, and monitoring functions.