Browse FAQs

What should be checked if an Altivar 61 or 71 display is showing NLP?

Published date: 16 December 2019

Issue:
Wondering what should be checked if an Altivar 61 or 71 display is showing NLP?

Product Line:
ATV61/71 drives

Environment:
All

Cause:
Drive displays 'NLP'

Resolution:
NLP indicates that no line power is present on the L1, L2 & L3 input terminals of the drive controller.

Check voltage at the L1, L2 & L3 terminals.
Check for open circuits on line contactors, circuit breakers, disconnect switches, or fuses.

If NLP state does not change with correct voltage present on L1, L2, & L3, remove the control board and check for loose connections of ribbon cables inside the drive.
WARNING: This step should be performed while the drive is powered down, and proper personal protective equipment should be worn. 

For example: In an ATV71HC25N4 a customer found a loose X3 connector from the control board to the board behind and above the control board. This connector was on a ribbon cable that was about 1 inch by 1 inch. Drive ran OK after this was reseated.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.