Browse FAQs

What causes an A17 fault on the ATS22 soft starter?

Published date: 26 November 2019

Issue:
A17 fault on the ATS22 soft starter?

Product Line:
Altistart ATS22

Environment:
All

Cause:
Keypad buttons are being held longer than 10 seconds

Resolution:
Try releasing the touch screen buttons.  Do not hold them more than 10 seconds.
Try swapping out the remote HMI keypad.  See if the problem follows the keypad or stays with the soft starter.
To reset the fault you have to power cycle the soft starter.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.