Browse FAQs

What is the maximum number of variables allowed in a Concept FBD section?

Published date: 26 November 2019


The maximum number of variables that may be used in an FBD section is 1899.

If more than 1899 variables are used in a section, Concept will generate the
following error:

You ( have ) reached the maximum number of Links allowed in a Section
Error Id: AI - 375

NOTE: The variables do not have to be unique instances, meaning, the same variable could be entered 1899 times.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.