Browse FAQs

Will the output of RS (Flip-flop,reset dominant) hold its value on a power down?

Published date: 12 December 2019

If the output is tied to an unlocated variable (memory address), on power down/up it will hold its value. If it is tied to a direct address or a located variable, after a power down/up it will be cleared to zero.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.