Browse FAQs

Can I tell what the Modbus Plus address of my Modicon PLC is via 984 ladder logic?

Published date: 22 November 2019

Yes, the contents of the address configured in node 2 of the MSTR Instruction Function Code #3 (Get Local Statistics) will give you the Modbus Plus Network address of the PLC.
Below is a example of a MSTR Instruction using Function Code #3 (Get Local Statistics) to get the Modbus Plus address of the PLC

400001 = 3 (Operation Type)
400003 = 1 (length)
400004 = 2 (Offset)
400010 = 2 (Network address of this station)


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.