Browse FAQs

Can I launch other applications from Control Expert (formerly Unity Pro)?

Published date: 26 November 2019

Yes, this can be done by choosing 'Customize' under <Tools>. Go to the 'Tools' tab and hit the 'Add' button and type in the name of the application in the 'Menu Text:'
Under 'Command' type in the path to the application. In the case of the Microsoft Event Viewer, this will be :
'C\windows\system32\eventvmr.exe'.
Hit <OK>. From the menu line, expand <Tools> and 'Event Viewer' will appear as a choice at the bottom of the drop down box. Clicking on Event Viewer will bring up the Microsoft Event Viewer which can be used to view the Audit Trail set up in the Unity Security Editor.

The example below adds the Microsoft Event Viewer:


Legacy KB System (APS) Data: RESL170094 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.