Browse FAQs

What is the purpose of the 'Add hyperlink' function in Unity Pro?

Published date: 16 December 2019

Hyperlink allows the user to create a link between the project and external documents or applications. Right click on a project section and choose 'hyperlink' to specify a document or application location. A link can also be added to the comment field in animation tables, data editor variables, operator screens and documentation.

When bringing in a Concept project, the message "cannot import hyperlink" message means that the document or application that was hyperlinked needs to be manually relocated from the Concept location to the Unity location.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.