Browse FAQs

What are the battery specifications for the Quantum PLCs?

Published date: 22 November 2019

Issue
Battery Specifications

Product Line
Modicon Quantum 

Resolution
The shelf life of the Quantum battery 990XCP98000 is 10 years with 0.5% loss of capacity per year. The same specifications applies to a PLC in the on condition 24x7.
With the PLC in the off condition, the battery will maintain the memory to the following PLCs as indicated:

140CPU11302 454 days
140CPU11303 238 days
140CPU21304 454 days
140CPU42402 238 days
140CPU43412X 238 days
140CPU53414X 119 days


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.