Browse FAQs

How to determine if a TCP/IP port is in use

Published date: 19 August 2020

Issue
It is unknown whether or not a certain TCP/IP is in use. 

Product Line

Power Monitoring Expert 2020
Power Monitoring Expert 9.x
Power Monitoring Expert 8.x
Power Monitoring Expert 7.x

Environment
Windows Operating System

Resolution
Open a Command Prompt running As Administrator and run "netstat -ano" (see below).



The first line under Local Address indicates that the local machine is listening on port 80 which is being used by Web Reporter. You can use the (Process ID) PID to locate the service or application that is using that specific port.



The following web page explains in detail how to interpret the netstat -ano results.

http://www.dti.ulaval.ca/webdav/site/sit/shared/Librairie/di/operations/informatique/windows/netstat_results.htm


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.