Browse FAQs

Can you adjust the scaling of the axes in a trend report in web reporter?

Published date: 18 December 2019

Product Line
Power Monitoring Expert

Environment
Web Applications

Resolution
No it cannot be done. The trend report under web reporter is auto-scaled depending upon the data and cannot be customized. Customizing these reports will require custom programming and it will have to be purchased. The report developer kit used to create custom reports is not available for end users, it is given only to integrators. One work around is to export the data in excel and then generate a whole new report according to one's preferences.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.