{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Error When Installing ION Enterprise 5.6 SP1

Goals and Symptoms

Summary
When running build 552 of ION Enterprise 5.6 Service Pack 1, the installer quits with the following error message:


This message appears when a user is attempting to run the latest version of the 5.6 SP1 installer on a server that is already running ION Enterprise 5.6 SP1 Build 549.

The specific build version may be viewed by selecting Help > About from any ION Enterprise application (e.g. ION Management Console, ION Vista, ION Designer). The about box on a server running ION Enterprise 5.6 SP1 Build 549 will appear as shown below:

Facts and Changes

Keywords
Error -1646 Uninstallation of the patch package is not supported

5.6 SP1 install

Causes and Fixes

Cause
It is not possible to update Service Pack 1 build 549 to Service Pack 1 build 552 by running the build 552 Service Pack 1 installer.

Resolution

Run the ION Enterprise 5.6 SP1 hotfix, which is attached to RESL190756. That hotfix incorporates all of the changes that were introduced between build 549 and build 552.

More Information

To verify that the hotfix has been installed on a server, go to the SetupLogs folder and look for a file named Hotfix_Setup.log. This file is created by the hotfix installer.


Last Revised: January 29, 2008

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL190866 V1.0, Originally authored by DeCr on 01/30/2008, Last Edited by DeCr on 01/30/2008
Related ranges: ION Enterprise V5.6