Browse FAQs

What causes a "Ladder Logic Mismatch Absolute Network 1. Segment 1 is not in database" error when connecting to a PLC with Concept?

Published date: 12 December 2019

This error message can be generated if the PLC had previously been logged into using ProWORX NxT. ProWORX NxT inserts an empty network at the start of logic.
This error must be corrected by performing a full project download using Concept.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.