Browse FAQs

Can the Twido support an SSI absolute encoder?

Published date: 11 November 2019

Issue:
Can an absolute encoder be used with an SSI absolute encoder? 

Product Line:
Twido

Environment:
TwidoSoft, TwidoSuite

Cause:
Looking to see if you can use a SSI absolute encoder with a Twido.

Resolution:
No, the Twido does not support the SSI absolute encoder. The Twido will support one of the following, up/down, up/down 2 phase counter, single up, single down, frequency meter.

Note: The Twido product line was obsolete 12/31/2016 and has been replaced by the M221 product line.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.