Browse FAQs

Why is my M1E not IO scanning my Advantys STBNIP2212 island?

Published date: 10 January 2020

Issue:
How do you I/O scan and Advantys STB Ethernet Island?

Product Line:

Momentum, Advantys STB

Environment:

Concept, Proworx, Advantys configuration software

Cause:

Unable to read any of the resisters on the Advantys island.

Resolution

Ensure that the ethernet network, IP addresses and subnet masks are configured properly and all devices can be pinged.  Now verify that in the M1E IO scanner setup that the 'Read Ref Slave' memory location is set for 45392 and not 40001 as would be the case if scanning a Momentum IO base with an ENT communication adapter.  This is a common error with Advantys STB.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.