Browse FAQs

Does Unity Pro run on Windows 2008 Server?

Published date: 13 December 2019

Unity Pro v8 will run on Windows 2008 Server R2, standard edition, SP1.

Windows 2008 Server allows two users to run Unity Pro via a Remote Desktop Connection.

Only one user may be connected to the simulator at any given time.    If more than one user tries
to connect to the Unity Pro simulator, an error message is returned. ("Can't start Comm. Server.  Port 502
is already in use.")

Each user running Unity Pro will be able to connect to any supported PLC.

The type of license purchased will depend on how many users are running Unity Pro at the same time.
The Remote Desktop sessions will not have to authorize Unity Pro. 
Authorizing the installation running on the Windows 2008 server PC is sufficient.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.