Browse FAQs

Preset the Energy values on an ION 7700

Published date: 13 November 2019

Issue
Can the energy values on an ION 7700 meter be preset to a desired value.

Product line
ION 7700

Environment
All versions of ION 7700 firmware

Cause
The feature to edit an output register created for the ION 83/84/8500 meters was not ported to the ION 7700 meter.

Resolution
It is not possible to preset the energy value. Currently the only way to change the energy value is to reset to 0.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.