{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Can the remote keypad of the S-Flex drive be removed without interrupting the drive operations?

Issue:
Removing the remote keypad with the drive running.

Product Line:
Altivar 212, S-Flex

Environment:
All models

Cause:
None

Resolution:
Under typical Remote mode operation, removing the keypad while the VFD is running the motor will not interrupt the operation of the drive.

Two scenarios that will result in an Err9 fault when the keypad is removed are:
1) if running the VFD in Local mode
2) if the VFD is programmed for PID control and the setpoint source is FMOd=3

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.