Browse FAQs

What causes Concept error "807 Wrong controller type selected"?

Published date: 17 December 2019

Issue:
   Error message is displayed when trying to connect to the PLC.

Cause:
   The configuration of the project is not compatible with the PLC.

Resolution:
   1/  Make sure that the PLC chosen in the Project's PLC type configuration matches that of the target PLC.
   2/  Make sure that the type of firmware (IEC or LL984) in the PLC is the same as the firmware type of the Project's PLC.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.