Browse FAQs

Are the ATV61 and ATV71 flange kits rated to be mounted inside an NEMA 4 4X enclosure?

Published date: 25 November 2019

Issue:
Are the ATV61 and ATV71 flange kits rated to be mounted inside an NEMA 4  4X enclosure?

Product Line:
Altivar ATV61 and ATV71 with the optional Flange kits

Environment:
All

Cause:
Wants to know if the optional flange kits are rated for an NEMA 4 4X enclosure.

Resolution:
The flange kits VW3A9501 thru VW3A9515 are not rated to be mounted inside an NEMA 4/4X enclosure.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.