Browse FAQs

Does the CIC(controller inside card) used with ATV61/ATV71 drives have a built in battery back up?

Published date: 28 November 2019

Issue:
The controller inside card parameters have reset to factory default, does this CIC card have a built in battery back up?

Product Line:
ATV61/ATV71

Environment:
All

Cause:
N/A

Resolution:
The CIC does have lithium battery for back up.  This battery is designed to last up to 8 years.
Battery Data:  Timekeeper Snaphat M4T28-BR12SH1  (48mA

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.