Browse FAQs

How can one application be distributed to multiple HMI's easily at once

Published date: 20 December 2019

Issue:
Looking for a method to send an application update to multiple HMI's in one easy command.

Product Line:
Vijeo Designer (all versions)

Resolution:
One option to satisfy such a requirement would be to use the Self download feature of Vijeo Designer. Please see the Online Help section 25.6.9 Self Downloading to Target Machines for more details. Essentially a single application is stored on a server and all the HMIs will connect to it to update automatically periodically or on demand or by trigger in an action.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.