Browse FAQs

How is the ATV71 R2 relay assigned to a brake logic function?

Published date: 25 November 2019

Issue:
How do I assign R2 to a brake logic function?

Product Line:
ATV71

Environment:
All

Cause:
VFD needs to control an electromechanical brake.

Resolution:
When the brake logic function is used, a VFD output needs to be assigned to control the brake release/engage.  This is done with a relay or logic output.  The brake logic function is activated when the brake assignment is made.

Main Menu
Drive Menu
1.7 Application Function
Brake Logic Control
Brake assignment  set to R2

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.