Browse FAQs

How do I install Vijeo Designer to be used under a Non-Administrator account in Windows?

Published date: 21 December 2019

Issue:
Looking for information regarding using Vijeo Designer on a non-Administrator account.

Product Line:
Vijeo Designer

Resolution:
There are two scenarios to consider for this question.

1) Versions Prior to Vijeo Designer V5.1
2) Versions from Vijeo Designer V5.1 and up.

In case 1, Vijeo Designer V4.6 - V5.0 will require you to make a selection during installation to specify if you want All users to use Vijeo Designer or just the Adminstrator. There will be a selection provided during the installation wizard.

In case 2, Vijeo Designer V5.1 and up will automatically install and configured Vijeo Designer to run under any type of Windows account. There is nothing specific that needs to be done.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.