{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Setting up permissive function on the ATV61 and ATV71 drives?

Issue:
On the ATV61 and ATV71 drives how can you add another run permissive input if you already have freewheel stop assigned?

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
There are several options of adding another run permissive on this drive.
- You can remove the factory jumper and tie in your stop circuit between the PWR and +24 terminals
- You can assign a Fast Stop as a logic input
  - Drive Menu ~> 1.7 Application Function Menu ~> Stop Configuration ~> Fast Stop Assignment
- You can use an External Fault with either Normally Closed or Normally Open set of contacts
  - Drive Menu ~> 1.8 Fault Management Menu ~> External Fault ~> External Fault Assignment