Browse FAQs

What is the S06 option on the S-Flex 212 Drive?

Published date: 03 January 2020

Issue:
S06 option on the S-Flex 212 Drive.

Product Line:
S-Flex 212

Environment:
All serial numbers for S-Flex 212

Cause:
N/A

Resolution:
The S06 option is for Seismic Certification
Seismic Certification:
• IBC, NFPA 5000 and ASCE7
• ICC ES AC 156

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.