Browse FAQs

Why is the sample rate for the Historical Trend graph stuck at 1 / s ?

Published date: 27 November 2019

Issue:
When using Triggered Data Logging, the Trend Graph still shows that the sample rate is 1 sample per second.

Product Line:
Vijeo Designer

Resolution:
When using the the Historical Trend Graph with a Data Logging Group that is setup with a trigger, you must set the TimeAxisRange property of the Trend Graph to be Time rather than NumOfSamples. For triggered data logging, the default settings will give you only 1 sample / second for the triggered data logging group.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.