{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Is there a document that explains the setting up of RSTP on the Connexium switches?

Issue
A document that explains the setting up of RSTP on the Connexium switches

Product Line
Connexium

Environment
Control Expert

Resolution
Attached is a document that explains setting up RSTP on the Connexium switches.
To create a RSTP ring, you will need to activate RSTP and assign RSTP to the required ports on each Connexium switch.
Note: For RSTP to work properly, all switches in the RSTP ring must have RSTP activated on the ports used to connect them together.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.