{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Osisense XC special - Special XCRF1435687 limit switch datasheet

Please note that the special XCRF1435687 limit switch is not shown into the Osisense XC Special limit switches catalogue, i.e. any data sheet does not exist. It is in fact the standard XCRF17 limit switch, supplied with 2 square rods 6mm, 200mm lenght both. The standard XCRF17 switch is supplied with 2 square rods 6mm, 200mm (XCRZ03) & 300mm (XCRZ04). Attached standard XCRF17 dimensions.

Explore more
Explore more