{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Can the Modicon M580 IO Scan nodes on different domains?

Title
 Modicon M580 IO Scan nodes on different domains
 
Issue
 Modicon M580 IO Scan nodes on different domains
 
Product Line
M580
 
Environment
Unity Pro 11.1
 
Cause
N/A
 
Resolution
 It is not possible to IO Scan devices that are located on different domains with the M580 built-in Ethernet port or the BMENOC0301.2 module. Unity pro will display an error saying both IP and gateway should have the same subnetwork mask. To IO Scan devices in different domains requires the use of a BMENOC0301.3  with Unity pro V11.1.
 
Explore more
Explore more