Browse FAQs

Where can I find the Global Event Log option in Vista for PME 9.0 and PME 2020?

Published date: 13 January 2020

Issue
In PME 2020 and PME 9.0 the Global Event Log option is not located in Vista under the Edit tab

Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
PME Global Event Log

Resolution
Global Event Log button was removed in PME 9.0 and it was replaced with Alarm Viewer located in Web Applications. For more information see the Power Monitoring System Guide (Link below)

https://www.se.com/ww/en/download/document/PowerMonitoringExpertSysGuide/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.