Browse FAQs

ION9000 default IP address, username, and password

Published date: 20 December 2019

Issue
The default IP address, username, and/or password are needed for connecting/configuring the ION9000.

Product Line
ION9000 series 

Environment
Web server

Resolution
The default IP address is 169.254.0.10

The username and password are defined by the meter’s security configuration; if standard security is enabled, the password is the same as the front display password. Below is a list of the default usernames and passwords for standard and advanced security.

Default standard security mode username: 9000
Default advanced security mode username: User1, User2, User3, etc. 
Default standard and advanced security mode display password: 0.

Note: To help increase the security of your meter’s configuration and data, configure the meter’s username and passwords to be different from the default values.

For more information about the ION9000 series meter, please refer to the User Guide that can be downloaded at the link below:
ION9000 User Guide

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.