Browse FAQs

Where do I find the Runtime Installation files for EcoStruxure Operator Terminal Expert for my iPC?

Published date: 15 November 2019

Issue
I've installed my EcoStruxure Operator Terminal Expert Buildtime Configuration software on my office PC or laptop. Where do I get the Install files for the iPC running as an HMI?

Product Line
EcoStruxure Machine Operator Expert

Environment
Harmony iPC or Standard PC running Windows Embedded 7 or Windows 10

Resolution
For EcoStruxure Operator Terminal, the Runtime can be installed from the same installer package as the Buildtime installer.
  1. Run the installer on your iPC (or the PC you intend to use as an HMI),
  2. Click Next from the first screen.
  3. In the second screen, the "Select Features" screen you will see two checkboxes
  4. Untick the "EcoStruxure Operator Terminal Expert" checkbox (this is the Buildtime component).
  5. Tick the "EcoStruxure Opeterator Terminal Expert Runtime" checkbox.
  6. Click Next and follow the instructions from the Installer screens.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.