Browse FAQs

Are the HMIBMI and HMIBMO iPCs supported in EcoStruxure Machine Operator Terminal Expert?

Published date: 15 November 2019

Issue
In EcoStruxure Machine Operator Terminal Expert configuration software, I do not see a Target selection for Harmony Edge Box series iPCs with prefixes HMIBMI or HMIBMO. Can I still use them as HMI running EcoStruxure Machine Operator Terminal Expert?

Product Line
EcoStruxure Machine Operator Terminal Expert, Harmony Edge Box iPC

Environment
HMI Configuration software in Windows

Resolution
The HMIBMI and HMIBMO Harmony Edge Box series iPCs are not marketed to be in the EcoStruxure Machine Operator Terminal Expert domain of HMIs, however, it can still be used.

You will need to choose the standard “PC/AT” Target Type to download to the HMIBMI or HMIBMO unit.
Also, you will need to match the desired screen resolution in the selection screen of what is set from the video driver of your device.

Note the license part numbers for EcoStruxure Machine Operator Terminal Expert Runtime are:
HMIRTWCZLSPAZZ – Runtime Emailed License
HMIRTWCZLSPMZZ – Runtime Printed License

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.