Browse FAQs

What is the recommended size of the fast blow fuse needed for the BMXSDI1602?

Published date: 19 November 2019

Issue:
Unable to find information regarding the size of the fast blow fuse needed for the BMXSDI1602.

Product Line:
x80, BMXSDI1602

Resolution:
According to the Modicon M580 Safety Manual, (see attached PDF), on page 66, it states that the recommended fast blow fuse to use with the BMXSDI1602 is 0.5 A.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.