Browse FAQs

Can EcoStruxure Control Expert co-exist with Unity Pro on the same PC?

Published date: 21 November 2019

Issue:
Looking for a way to keep both EcoStruxure Control Expert and Unity Pro installed on the same PC. Is it possible to keep both versions?

Product Line:
EcoStruxure Control Expert, Unity Pro,

Resolution:
When installing EcoStruxure Control Expert on a PC that already has Unity Pro installed, the installation process will automatically remove Unity Pro. Therefore, it is not possible to have both Unity Pro and EcoStruxure Control Expert on the same PC. The only possible solution is to have a separate Virtual Machine for Unity Pro and EcoStruxure Control Expert.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.