Browse FAQs

Any restrictions on the subnet mask or gateway communications for the ADVC-2 Controller?

Published date: 11 December 2019

Issue
What subnet blocks (/29, /30, /31) are supported on the NuLec ADVC2 platform when connected to an ethernet/IP port?

Product Line
ADVC-2 Controller

Environment
Operations Manual, Communication

Resolution
No restrictions on subnet or on the gateway for the ADVC-2 Controller.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.