Browse FAQs

Can the Harmony HMISTW browser HMI be used in Portrait mode

Published date: 04 December 2019

Issue
Is the Harmony HMISTW dedicated browser HMI mountable and viewable in Portrait (vertical display) mode instead of Landscape (horizontal display)?

Product Line
Harmony HMISTW (browser HMI)

Environment
Physical Human Machine Interface (HMI) touchscreen panel

Resolution
No, the Harmony HMISTW series HMI do not support display in Portrait mode. Only Landscape mode is supported.

Note that the HMIST6 (no 'W') series which is configured in EcoStruxure Operator Terminal Expert (previously known as Vijeo XD) supports rotation of some (not including the Trend Graph, Recipe Manager, Alarm Summary) objects (+90, -90 and +180 degrees) from the Screen menu bar so that some screens can be used in Portrait (vertical) view as well as other orthogonal orientations. The HMISTW series is only configurable as a dedicated web-browser HMI and is not configured with EcoStruxure Operator Terminal Expert.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.