Browse FAQs

Can the ATV320 be used with Ring Topology when connected with the VW3A3616 Ethernet Card?

Published date: 11 December 2019

Issue:
Can Ring Topology be used on the ATV320 drive connected with the VW3A3616 Ethernet Card?

Product Line:
ATV320

Environment:
All model numbers

Cause:
Customer would like to use ring topology with the ATV320 drive.

Resolution:
No, Ring topology is not supported by the ATV320.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.