Browse FAQs

Can the VW3A1111 keypad be used with other foreign drives?

Published date: 11 December 2019

Issue:
Is the VW3A1111 keypad compatible with foreign drives?

Product Line:
ATV630 ATV930

Environment:
N/A

Cause:
Customer asked if the keypad VW3A1111 can be used with Toshiba drive.

Resolution:
No, because keypad's software and feature are not compatible with foreign drives.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.