Browse FAQs

Which HMI part numbers are supported in EcoStruxure Operator Terminal Expert v3.1 SP1?

Published date: 14 January 2020

Issue
What are all the models of HMI that can be programmed with EcoStruxure Operator Terminal Expert v3.1 SP1?

Product Line
EcoStuxure Operator Terminal Expert

Environment
HMI Configuration

Resolution
The following is a list of all the supported HMI families and models:
Family Model Attachable Screen
HMIST6 HMIST6200 (4.3" Wide) -
HMIST6400 (7" Wide) -
HMIST6500 (10" Wide) -
HMIST6600 (12" Wide) -
HMIST6700 (15.6" Wide) -
HMIGTU HMIG3U HMIDT351 (7" Wide)
HMIDT542 (10.4")
HMIDT551 (10" Wide)
HMIDT642 (12.1")
HMIDT643 (12.1")
HMIDT651 (12" Wide)
HMIDT732 (15")
HMIDT752 (15" Wide)
HMIDT952 (19" Wide)
HMISTO HMISTO705 (4.3" Wide) -
HMISTO715( 4.3" Wide) -
HMISTO735 (4.3" Wide) -
HMIBM* All families:
HMIBMI
HMIBMO
HMIBMU
HMIBMP
HMIDM6421 (12")
HMIDM6521 (12" Wide)
HMIDM7421 (15")
HMIDM7521 (15" Wide)
HMIDM9521 (19" Wide)
HMIDMA521 (19" Wide)
HMIPS** HMIPSO*5 (10") -
HMIPSO*7 (15.6") -
HMIPSP*7 (15.6") -
HMIPSP*9 (18.5") -
HMIPEP*9 (18.5") -
HMIBU** Series HMIBUCND1E01  
HMIBUFND1P01 -
HMIBUFND1PF1 -
HMIBUFND2P01 -
HMIBUFND2PF1 -
HMIBUHND1P01 -
HMIBUHND2P01 -
HMIBS** Series HMIBSO0ND1001  -
HMIBSOCND1E01 -
HMIBSU0ND1001 -
HMIBSUCND1W01 -
HMIBSUSND1W01 -
HMIRS** Series HMIRSOHPA3W01 -
HMIRSPFXA6701 -
HMIRSPFXR6702 -
HMIRSPHXA6701 -
HMIRSPHXA67P1 -
HMIRSPSXR6S01 -
HMIRSPSXR6T01 -
HMIRSPSXR6T01 -
HMIRSUS3A3701 -
HMIPW*5** Series HMIPWC5D0E01 -
HMIPWC5D0E01A -
HMIPW*7** Series HMIPWC7D0E01 -
HMIPV*7** Series HMIPVC7D0E01 -
HMIPU*6** Series HMIPUF6A0701 -
HMIPUC6A0E01 -
HMIPUF6A0701 -
HMIPUF6D0701 -
HMIPP*6** Series HMIPPF6A2701 -
HMIPPH6A2701 -
HMIPU*7** Series HMIPUC7D0E01 -
HMIPUF7D0P01 -
HMIPUF7D0PL1 -
HMIPUF7A0P01 -
HMIPUH7D0P01 -
HMIPUH7A0P01 -
HMIPUF7A2P01 -
HMIPUF7A2PF1 -
HMIPUH7A2P01 -
HMIPUH7A2P01 -
HMIPT*7** Series HMIPTF7D2P01 -
HMIPTH7D2P01 -
HMIPP*7** Series HMIPPF7D0701 -
HMIPPF7D07F1 -
HMIPPH7D0701 -
HMIPPH7A0701 -
HMIPPF7A2701 -
HMIPPF7A27F1 -
HMIPPH7D2701 -
HMIPPH7B2701 -
HMIPPH7A2701 -
HMIPR*7** Series HMIPRH7A2701 -
HMIPU*9** Series HMIPUC9D0E01 -
HMIPUF9D0P01 -
HMIPUF9D0PF1 -
HMIPUH9D0P01 -
HMIPUH9A0P01 -
HMIPUF9A2P01 -
HMIPUF9A2PF1 -
HMIPUH9D2P01 -
HMIPUH9A2P01 -
HMIPP*9** Series HMIPPF9D0701 -
HMIPPF9D07F1 -
HMIPPH9D0701 -
HMIPPH9A0701 -
HMIPPH9A0701 -
HMIPPF9A27F1 -
HMIPPH9D2701 -
HMIPPH9A2701 -
PC/AT Generic Windows PC -

Supported resolutions for iPCs / PCs:
320x240 (QVGA)
640x480 (VGA)
800x480 (WVGA)
800x600 (SVGA)
1024x768 (XGA)
1280x800 (WXGA)
1280x1024 (SXGA)
1366x768 (FWXGA)
1440x900 (WXGA+)
1600x900 (WXGA++)
1920x1080 (FHD)
1920x1200 (WUXGA)
3840x2160 (UHD/4K)

Changes from EcoStruxure Operator Terminal Expert v3.1:
HMIGTO series is not supported in this version
HMIGTU Open Box (HMIG5U/HMIG5U2) is not supported in this version.
Windows-based iPCs are consolidated into the "iPC or PC/AT" category

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.