Browse FAQs

Is the USB stick that comes with the HMIBM series bootable?

Published date: 09 January 2020

Issue:
When looking at the instructions to start the recovery process of an HMIBM series, it states to backup the Recovery USB media. Do we need to make the destination USB Bootable?

Product Line:
HMIBM series

Resolution:
The USB restore media that comes with the HMIBM series is indeed a bootable device. However, if you copy the files to another USB media, it will be sufficient to make the destination USB media bootable as well. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.