Browse FAQs

How do I limit motor torque on Lexium 28 ?

Published date: 14 January 2020

To limit the motor torque on Lexium 28 simply lower the maximum motor current parameter ILIM found at parameter P1-78.

P1-78 sets the limit of the current that the drive will deliver to the motor.
Motor torque is proportional to motor current, so by lowering the current the available maximum torque will be limited.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.