Browse FAQs

ATS48 Can use 120Vac for a start / stop command?

Published date: 10 January 2020

Issue: 
Can the ATS48 use 120Vac for a start / stop command?

Product Line:
ALTISTART 48

Environment:
All serial numbers
 
Cause:
Installation / Setup

Resolution:
No,120Vac , 
Logic input voltage is +24Vdc. 
ATS48 generates the +24Vdc  power supply.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.