Browse FAQs

Which displays for the HMIGTU/HMIGTUX series supports multi-touch gestures?

Published date: 15 January 2020

Issue
Which displays for the HMIGTU/HMIGTUX series supports multi-touch and pinch-to-zoom gestures? What software is required?

Product Line
Harmony HMIGTU, Harmony HMIGTUX, EcoStruxure Operator Terminal v3.1

Environment
Physical touchscreen HMI

Resolution
The displays with the designation "Smart Display" support multi-touch and pinch-to-zoom gestures.
Part Numbers:
HMIDT732 (15" Touch Smart Display XGA)
HMIDT542 (10.4" Touch Smart Display SVGA)
HMIDT642 (12.1" Touch Smart Display XGA)

Note that only HMIGTU/HMIGTUX panels running EcoStruxure Operator Terminal Expert v3.1 support this feature. This is not supported in HMIs running Vijeo Designer Runtime.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.