{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Osisense XC - Datasheet of the adapted limit switch XCMD3902T1

Please find attached the datasheet of the adapted limit switch XCMD3902T1, using a special cable halogen free for railway equipments (1m cable length), complying to EN 50306 and EN 45545 standards. This reference is available to order without any restriction in 2022. It is not in stock, it is produced at order reception by the assembly plant.

Attachment(s)

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.