Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Can I download to a Harmony/Magelis HMISTU 655/855 using a mini-USB cable from Vijeo Designer?

Issue

Is it possible to download an application configured in Vijeo Designer Buildtime software to a Harmony (previously branded Magelis) HMISTU with Part Numbers HMIS5T, HMISTU655, HMISTU855 using a USB-A to USB Mini-B cable?

Product Line

Harmony or Magelis branded HMISTU Family

Environment

Physical Human Machine Interfaces

Resolution

Yes, the Vijeo Designer HMI application can be downloaded using a USB A to USB Mini-B cable.

The recommended Schneider Electric catalog number for that cable is BMXXCAUSBH018 (1.8m long) or BMXXCAUSBH045 (4.5m long)
It uses the XBTZG935 USB driver which is installed when Vijeo Designer Buildtime software is installed.