Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Compact Flash (CF) Cards Spares for the C3414 CPU

Issue:
Need to identify the correct spare part number for the Compact Flash (CF) memory card used with the C3414 CPU.

Product:
C3414 CPU, SAGE RTU Series

Environment:

  • Systems using C3414 CPU
  • Requires Compact Flash memory card for operation or replacement

Cause:
The CF card is a required component for the C3414 CPU, and users need the correct part number for ordering or replacement.

Resolution:
The part number for the required CF memory card is C3414-S02-10001.
Description: COMP FLASH 1GB W/FW&WLIC.